STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32F756 Ethernet and lwIP Rx and Tx Descriptor

Hello,I am creating a new project using STM32CubeIDE to use lwIP with internal MAC for a Nucleo F756 Board. When I enable the Eth peripheral, I can configure the Rx and Tx descriptors. They are placed at the start of SRAM2 (0x2004C000).Since the Cube...

descriptors.png descriptors.png new_region_sram2.png new_region_sram2.png

HAL RTC SetDate Bug or some another way to do??

Posted on February 23, 2017 at 10:49I am using STM32F103 in my new application. I have used STM32Cube to generate my code including Internal RTC. Myproblem is that the time is ok saved when reseted but date is always reset. when i inspected the code...

Output Compare Register update in stm32

I had taken TIM1 asn Master to Trigger TIM8 here below i had attached the timer configuration Clock Frequency 480mhz ,timer clock 240mhzHere Iam Triggering The TIM8 after 2.5us started from TIM1 both are 100khz frequency in TIM->CCR3 register iam loa...

IMG20250205175541.jpg IMG20250205175611.jpg IMG20250205175558.jpg

STM32CubeMX: TSC Advice

Well I got the new board back it seems to work, but it's quite different: I have 3 groups of 3 sensors and one group used for the shield. Previously Cube MX defined this as 3 Banks, now it has defined 6 Banks. Should I worry about this? In the first ...

Lanceh by Associate III
  • 1394 Views
  • 3 replies
  • 0 kudos

Difference in Generated Files: STM32Cube.AI GUI vs. CLI

When generating code using STM32Cube.AI GUI, I get all the necessary project files.However, when using the CLI, I only get the model's .c and .h files. Is there a command to generate all the additional files via CLI? Or can anyone explain the differe...

mkothuri by Associate II
  • 1058 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.