STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

stm32u575 & Ethernet support On CubeMx

A new question moved from this thread to the correct forum board (to be answered by CubeMx team) Hi If STM32U5 has no support for Ethernet why in configurator i can enable the Middleware NetxDuo?  The question start from this point, NetxDuo support, ...

mauroalba by Associate II
  • 4830 Views
  • 1 replies
  • 0 kudos

Resolved! CubeMX BUG: Setting LSE Drive Capability

Posted on October 17, 2017 at 12:08When using CubeMX, with STM32L476, for setting LSE drive capability other than 'Low Drive' the setting will not be implemented. This is due to the fact that the write access using bit DBP in PWR->CR1 is not set pri...

Feature Request - Pin selection - CubeMx

Hello,When a user adds a peripheral (for example I2c),  CubeMx picks some default and/or available pins for the device.It would be really nice if CubeMX can list all the Alternative pins that this peripheral can use.  So by right clicking on "I2C_SCL...

mattcrc_0-1741334003863.png
matt-crc by Senior III
  • 1354 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.