2019-11-25 8:55 AM
Hello,
can we change the sampling frequency on standalone mode for the X-NUCLEO-LPM01A without using any computer?
If I understand right, by default the sampling frequency is 100Hz, and I would like to increase it to 10khZ.
David
Solved! Go to Solution.
2019-11-28 8:13 AM
Hello David,
In standalone mode, the raw sampling frequency is fixed to maximum: 3.2Msamples/sec (this high frequency allows to catch short current peaks), then current is averaged: this is the configurable setting of integration time of few seconds.
In mode connected to computer, the raw sampling frequency is the same, the configurable setting of acquisition frequency is a subset of this frequency (averaged at 100kSamples/sec, then samples picked up).
Best regards
Philippe
2019-11-28 8:13 AM
Hello David,
In standalone mode, the raw sampling frequency is fixed to maximum: 3.2Msamples/sec (this high frequency allows to catch short current peaks), then current is averaged: this is the configurable setting of integration time of few seconds.
In mode connected to computer, the raw sampling frequency is the same, the configurable setting of acquisition frequency is a subset of this frequency (averaged at 100kSamples/sec, then samples picked up).
Best regards
Philippe
2019-11-29 12:14 AM
Hello Philippe,
thank you for answer, this one and the two other one, it helps a lot!
David
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.