2023-03-10 2:14 AM
Hello,
I would like to trigger a STM32 device reset from inside STM32CubeMonitor.
I'm developing an application using STM32CubeIDE and STM32CubeMonitor. Duringe measuring of my variables via STM32CubeMonitor it is possible that my device gets into a reduced function safe state (on purpose). Then it would be very helpful to trigger a device reset via a button like I'm able to do during debugging in STM32CubeIDE.
I understand currently only the topics: Read, Start and Stop are available for a probe-node. Is it possible to trigger a reset via additional (maybe undocumented) options or is this feature planned in a future release?
If not is there a workaround available? I tried to connect to the GDB server opened by the probe-node after starting the acquisition but wasn't successful. As far as a saw it, the server is always opend on a different port?!.
Thank you
Best regards
Martin
Solved! Go to Solution.
2023-03-30 12:37 AM
Hello @MKori.1
There's no such option in STM32CubeMonitor, as a workaround you may also try to use write node in order to write a variable to trigger an event in your application to reset.
2023-03-28 1:50 AM
As a workaround I can trigger a reset via STM32ProgrammerCLI. But this doesn't work when the connection is active.
2023-03-30 12:37 AM
Hello @MKori.1
There's no such option in STM32CubeMonitor, as a workaround you may also try to use write node in order to write a variable to trigger an event in your application to reset.
2023-03-30 2:18 AM
Hello,
thank you for your idea, this should work for me. As the debugger interface in the background is already able to reset the device is it planned to update the probe-node? Is there a place to post such ideas? Something like "Issues" in Github.
2023-03-30 5:33 AM
I will raise a Change request to the dev. team to post your proposal.
2024-11-25 8:56 AM
2024-11-27 5:34 AM
Hi @MKori.1 ,
No update for the Sw reset implementation unfortunately, I try to push to get it in nest 1.10 release.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.