2020-06-20 12:45 PM
Dear all,
is it possible to change the Y scale for Chart? In the information panel I can see group
[Home] Chartorder4
width"7"
height"5"
chartType"line"
curveType"linear"
duration"10"
ymin""
ymax""
, but in the Properties tab I can see only group, size, chart type, curve type, duration and name... Scale is missed.
Solved! Go to Solution.
2020-06-22 2:34 AM
Dear @OVeli.1 ,
These ymin & ymax attributes are only available for Bar chart type :
" Y-Axis : Allows to define the Y axis lower and upper bounds for a bar chart. If the min and/or max value(s) is (are) not set, the bar chart will autoscale to any values received (with the 0 value centered in the middle of the graph). "
If you select the chart type Bar chart, you will see attributes Y-Axis.
2020-06-22 2:34 AM
Dear @OVeli.1 ,
These ymin & ymax attributes are only available for Bar chart type :
" Y-Axis : Allows to define the Y axis lower and upper bounds for a bar chart. If the min and/or max value(s) is (are) not set, the bar chart will autoscale to any values received (with the 0 value centered in the middle of the graph). "
If you select the chart type Bar chart, you will see attributes Y-Axis.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.