2020-04-07 7:46 PM
Hi I am using STM32G431 and last version of CubeIDE.
When I am debugging on ADC12 Common resistor, It's address is 0x50000200.
The address should be 0x50000300.
How can I change that address?
Or Can you change it?
2020-04-07 7:56 PM
It's defined in stm32g431xx.h. Make sure you're including the right file. Appears to be correct:
#define ADC12_COMMON_BASE (AHB2PERIPH_BASE + 0x08000300UL)
2020-04-08 2:07 AM
Thank you for your answer. But I am talking about SVD File.
Anyway I found that file below link.
https://github.com/posborne/cmsis-svd/
and I changed the base address of ADC12_COMMON_BASE.
Now I can debug without problem. I think ST should change SVD file.
2020-04-10 10:24 AM
Hi @khong.1 ,
Thanks for bringing the error to our attention. It is tracked internally.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.