2019-07-20 8:29 AM
2019-07-20 12:04 PM
For gcc compiler what you have is not a constant, it is expression. C++ accepts this.
Clang accepts this even in C mode.
-- pa
2019-07-21 6:31 AM
So how do I do this?
This is my first project using C and STM32. I am trying to learn the basics before actually using Cube/FreeRTOS. I am trying to create a definition header file that I tweak a few up front parameters based on what hardware I choose to use, and these definitions set everything up for me.
2019-07-21 6:40 AM
#define BIT 12u
#define BITon (0x1ul << BIT)Usually in C bits are defined as preprocessor defines. Look for example:
P.S. I hope You are not redefining MCU registers and their bits...
2019-07-21 7:39 AM
CAVEAT: Yes, I am redefining the wheel. I am trying to learn the basics before taking advantage of what others have already done. This is my "Hello" project.
Actually it does accept expressions. This compiles:
const int VAL = (0x123456 & (~(0x3<<12))) | (0x1<<12);
but if I put a predefined non-zero constant expression in it, it does not. (0x0<<BIT works, 0x1<<BIT does not)
Not all of the definitions I like to use are defined in the STM32 headers. Bit position isn't, an explicit bit on, bit off, single bit field mask is not:
#define BD(DEV,REG,BIT,POS) \
const uint32_t DEV ## _ ## REG ## _ ## BIT ## _P = POS ; \
const uint32_t DEV ## _ ## REG ## _ ## BIT ## _Off = 0x0 << POS ; \
const uint32_t DEV ## _ ## REG ## _ ## BIT ## _On = 0x1 << POS ; \
const uint32_t DEV ## _ ## REG ## _ ## BIT ## _M = ~(0x1 << POS )
BD(RCC,CR,HSEON,16);
BD(RCC,CR,HSERDY,17);
And I don't like using time typing long expressions. I seem to be using the following expression a lot. I would like to turn it into a macro but can't:
RCC->CFGR = (RCC->CFGR & (~RCC_CFGR_PLLMULL_Msk)) | RCC_CFGR_PLLMULL9;
Note I am looking for inline macro expansion versus function calls because of the function call overhead.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.