STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

What causes the strange behavior in SWO Data Trace/ ITM?

I am trying to gain some confidence using the SWO debug methodsbut I experienced some strange beavior what I cannot explain.1. I tried to send a 32 bit value though ITMPort1 in an inifiteloop and it works awhile but sometimes it switches to ITMPort21...

NCTUser by Associate III
  • 2198 Views
  • 0 replies
  • 1 kudos

Gcc optimization problem

I have a problem in STM32CubeIDE.​unsigned char readKey (void) { volatile unsigned char keyValue=HAL_GPIO_ReadPin (KEY_GPIO_Port, KEY_Pin); if (0 == keyValue) { printf ("before delay\r\n"); HAL_Delay (10); keyValue=HAL_GPIO_ReadPin (KEY_GPIO...

User.151 by Associate
  • 1555 Views
  • 2 replies
  • 0 kudos

How to Set Code Auto-Completion?

:sad_but_relieved_face: It`s my first time to use tools like STM32CubeIDE ( keil v5 before :) ). I want to know where can i set Code Auto-Completion or CODE-TIPS ?Thanks!

hbowe by Associate II
  • 6156 Views
  • 3 replies
  • 4 kudos

Debug error

SEGGER J-Link GDB Server V6.44c Command Line Version​JLinkARM.dll V6.44c (DLL compiled Mar 22 2019 17:26:40)​Command line: -port 2331 -s -device STM32F042F4 -endian little -speed 1000 -vd-----GDB Server start settings-----GDBInit file:         noneGD...

0690X000009YxB7QAK.jpg
hbowe by Associate II
  • 1431 Views
  • 1 replies
  • 1 kudos

stm32cubeide.exe gets deleted upon running

I've tried installing STM32CubeIDE for the first time on Windows 10. Every time I run it, it automatically closes, and the stm32cubeide.exe file gets deleted. I've reinstalled 1.0.0, 1.0.1 and 1.0.2 several times but this happens every time.Anyone fa...

KLe by Associate
  • 1463 Views
  • 2 replies
  • 1 kudos

Fatal error with bsp_driver_sd.h

Hi ST Community,as you see in the pic below I have a problem with bsp_driver_sd.hI created a new folder called Fatfs and in this folder a new one its name Core , I put the source file as shown, I ceated the header file (bsp_driver_sd.h) but i still d...

0690X000009Yx1HQAS.png
idrissmc by Associate III
  • 2015 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.