2020-09-10 6:05 AM
Hello everyone,
I recently bought a Nucleo-L4 board and I wanted to program it with CubeIDE on windows. The matter is each time I run the installer I have "NSIS error" telling me that it can run the installer. What other software do advice me to use ?
My windows is up to date and I can run other software installer without matters
Thanks in advance :beaming_face_with_smiling_eyes:
2020-09-10 6:16 AM
Check what kind of AV software you have running, and if that is blocking or interfering with installation.
Run As Administrator.
Check if you have Java JRE, and versions.
Try install into different directory.
Not sure if the installer generates a log file.
What version of Windows?
Consider pro tools like Keil or IAR
2020-09-10 6:51 AM
I use Windows 10. I have the las version of Java JRE.
Are these soft free ?
I also saw that Arduino could program st card. Does it work with Stm32L4 ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.