2021-01-21 2:58 AM
Hello everyone,
I want to debug an existing application (STM32F405) of my company which has been coded without IDE (so just makefile and gcc on our server) and using the stlink to flash.
I imported this project with the option "makefile project" on the CubeIDE and with small changes i made it compile. However i can't run debug and i get that error :
Error in final launch sequence:
Failed to execute MI command:
-exec-run
Error message from debugger back end:
During startup program exited with code 126.
Failed to execute MI command:
-exec-run
Error message from debugger back end:
During startup program exited with code 126.
During startup program exited with code 126.
Also i get an error which talks about mcu target not configured in build configuration but i don't see where i should select the target.
Anyway did someone dealed with that issue and fixed it ? I believed IF it's possible that i have to configure the build / debug configuration or sth else but i can't figure out what is exactly the problem.
Thanks in advance for your asnwer.
Best Regards,
Thomas
2021-01-21 3:15 AM
Think that the "makefile project" is for native projects running on the host, not cross-debugging.
2021-01-21 3:21 AM
Yeah thanks for the answer this is what i assumed after i got my error messages :grinning_face_with_sweat: but so what is the good way to do that ?
2021-01-21 5:15 AM
In fact my question could be : how to convert an externally build project into an STM32CUBE project ?
2021-01-21 7:36 AM
Now i succeeded ton compile it and start debugging session but can't add or edit my code while debugging (for example for live expression).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.