STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE 1.3.0 error: ST-LINK_gdbserver.exe not found

ST-LINK_gdbserver.exe disappeared from STM32CubeIDE:Error in final launch sequence:   Failed to start GDB server Failed to start GDB server Error launching GDB server. Session terminated Cannot run program "C:\ST\STM32CubeIDE_1.2.0\STM32CubeIDE\plugi...

Resolved! Using section attributes within a union

I've been assigning some of my storage areas into different memory areas as defined within the STM32H743ZITX_RAM.ld file in a project using STM32CubeIDE. This has first required me to insert the appropriate definitions where I've used memory domain D...

NSR by Associate III
  • 4934 Views
  • 5 replies
  • 2 kudos

Resolved! Timeout during download

New a project for generating code while install the STM32CubeIDE first time. I try to close my firewall but it doesn't work.

0693W000007BkL5QAK.png 0693W000007BkLPQA0.png
Gchen.1 by Associate II
  • 2765 Views
  • 4 replies
  • 1 kudos

Cube32CubeIDE v1.5.1 skips breakpoints

Hello everyone,​first of all, a 'hello' from me as I'm new to the STM-world! Today I sarted with the Cube IDE on Ubuntu and a STM32H743ZI2 NUCLEO board. After troubleshooting the IDE i finally managed to get it working. When debugging, the program is...

MLang.7 by Associate III
  • 1168 Views
  • 1 replies
  • 0 kudos

run release without breakpoints

Hi,I flash a project for debugging and set some breakpoints. Then I compile for release and run the code using the green arrow symbol. The code is flashed, but does not run, as it is stuck in a breakpoint from earlier debug sessions.Is there a way to...

How to use arm_sin_f32 and arm_cfft in STM32CubeIDE

I'm using arm_sin_f32 and arm_cfft in STM32CubeIDE, but no matter how I change my setting, there is still a bug like "undefined reference" exist. It seems like I have done wrong while changing the setting.Is there a user guidence of how to use these ...

KXu.3 by Associate II
  • 4011 Views
  • 5 replies
  • 1 kudos

Missing project builder/toolchain configurations in CubeIDE

I am trying to build my first STM32H7 project. I used CubeIDE (the MX module?) that seemingly works fine and generates the project code and source files using the default configurations. However, after opening the newly generated project, no C/C++ to...

SSohe.1 by Associate
  • 3762 Views
  • 2 replies
  • 3 kudos

Secure 'some' peripherals error from code generation

When I use STM32CubeIDE (version 1.5.0) to generate a new secure project for the STM32L562 Discovery Board.... I get a warning when I try and generate code from the device configuration. It says:It is recommended to secure some peripheral(s).And poin...

KHenr.1 by Associate
  • 771 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.