2025-03-31 3:07 AM
/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.macos64_1.0.0.202411102158/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld: warning: pedal13.elf has a LOAD segment with RWX permissions
When launching a build in my project (IDE C/C++) , I'm getting the above in the console window from the build.
Is this normal? Should I care?
Solved! Go to Solution.
2025-04-01 12:58 AM
This article explains what the warnings are, why they've "suddenly" started appearing, and what to do about them - including just disabling the warning:
https://www.redhat.com/en/blog/linkers-warnings-about-executable-stacks-and-segments
#rwxWarning
2025-03-31 2:25 PM
Usually you should care about warnings and unusual messages. This one can be ignored for many STM32 models because yes, the memory is defined in the linker scripts as RWX. If this annoys, change the attributes so that no memory block has W and X together.
2025-04-01 12:42 AM - edited 2025-04-01 1:12 AM
I'm a bit clueless where this is made. I can find a piece of code in
<project_name>.map (excerpt):
Memory Configuration
Name Origin Length Attributes
RAM 0x20000000 0x00005000 xrw
FLASH 0x08000000 0x00010000 xr
*default* 0x00000000 0xffffffff
Linker script and memory mapBut wouldn't it be normal to give RAM these attributes (rwx)?
Defined in the loader file:
STM32F103C8TX_FLASH.ld
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 20K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 64K
}
And I changed this to `rw` to no avail. The warning persists.
Would it be possible to increase the linker verbosity to find out which segment is the culprit?
2025-04-01 12:52 AM
This is defined in the linker script - the .ld file; eg,
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 8K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 64K
}
Remove the 'x' from RAM, if you wish
2025-04-01 12:58 AM
This article explains what the warnings are, why they've "suddenly" started appearing, and what to do about them - including just disabling the warning:
https://www.redhat.com/en/blog/linkers-warnings-about-executable-stacks-and-segments
#rwxWarning
2025-04-08 12:39 AM
Follow-on question about adding compiler options:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.