2019-05-27 11:43 PM
Hi I need some help,
I am having the same problem using CubeIDE v1.0. I have copied the arm_math.h, const_structs.h and arm_common_tables.h into Drivers/CMSIS/DSP/Include.
I was not able to find arm_math.h until I went to Project > Properties > C/C++ General > Paths and Symbols > Includes and added in Drivers/CMSIS/DSP/Include. That fixed the problem of not finding arm_math.h
After which I get a whole bunch of errors:
__uint32_t
../Drivers/CMSIS/DSP/Include/arm_math.h:6612:3: error: unknown type name 'uint32_t'; did you mean '__uint32_t'?
uint32_t blockSize);
...
...
../Drivers/CMSIS/DSP/Include/arm_math.h:6873:16: error: unknown type name '__STATIC_INLINE'
CMSIS_INLINE __STATIC_INLINE q15_t arm_bilinear_interp_q15(
^~~~~~~~~~~~~~~
../Drivers/CMSIS/DSP/Include/arm_math.h:6873:38: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'arm_bilinear_interp_q15'
CMSIS_INLINE __STATIC_INLINE q15_t arm_bilinear_interp_q15(
^~~~~~~~~~~~~~~~~~~~~~~
../Drivers/CMSIS/DSP/Include/arm_math.h:6951:16: error: unknown type name '__STATIC_INLINE'
CMSIS_INLINE __STATIC_INLINE q7_t arm_bilinear_interp_q7(
^~~~~~~~~~~~~~~
Thanks!
2020-04-01 2:42 PM
Step 1: Copy CMSIS/Drivers/DSP/ Include and Source folders like you already did
Step 2: Add /DSP/Include - folder to your include path settings
Step 3: under "Symbols" add TWO of them : a) ARM_MATH_CM7 (for M7 CPUs) b) __FPU_PRESENT (each of them without values)
Step 4: have Fun ;)
It seems, you missed step 4b ...
/Charly
2020-06-07 1:48 PM
I was getting a lot of errors as well, I tried many things and the most I achieved was to be able to have the #include "arm_math.h" in the file without generating compilation error, but I wasn't able to use any of the library functions.
I found a video and following the "Preparations" section [min 2:29-5:00] solved the issues to me.
This is the video:
https://www.youtube.com/watch?v=vCcALaGNlyw
Hope this helps
2020-06-27 11:29 AM
Thank You
This answer and video worked for me .
2022-05-15 8:55 AM
@weehong.yeo Just want to say a HUGE thank you for this thread. Spent hours struggling till I found your excellent description!
2022-05-16 6:39 PM
No prob! Glad it is helpful! :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.