2023-07-27 11:50 AM
Updated STM32CubeIDE version 1.11.0 to version 1.13.0
Using an St-LINK/V2 to connect PC to a prototype board with a STM32L476 on it.
STM32CubeProgrammer can load the debug .elf file and read the L476 memory just loaded.
The CubeIDE 1.13.0 does a clean build but when I select:
Run---Debug As---1 STM32 C/C++ Application----.elf file
I get the following error:
“No ST-LINK detected! Please connect ST-LINK and restart the debug session.”
The ST-LINK is connected. The Programmer just used it to load the .elf file.
2023-07-27 12:33 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.