2020-01-02 4:53 AM
Hi everybody!
Have problem with building project, which is OK in TrueStudio.
I have:
Core/Inc/font24.o:(.rodata.Font24_Table+0x0): first defined here
collect2: error: ld returned 1 exit status
make: *** [makefile:42: test3.elf] Error 1
"make -j7 all" terminated with exit code 2. Build might be incomplete.
15:42:59 Build Failed. 1 errors, 0 warnings. (took 151ms)
Tried to solve the issue with Builder setting, but this settings is unavailable under MacOS Catalina /STM32CubeICE
Could you pls suggest any solution?
Regards
Evgenii
2020-01-08 2:03 AM
Do you get that pop-up with every project you create or this specific one that worked in TrueSTUDIO?
Do you have a way to recreate the problem?
2020-01-08 3:35 AM
yes. Every project I've generated I had this pop up message.
2020-01-08 6:03 AM
Seems like I get the same thing after some testing. I'll write a ticket about it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.