2020-02-03 1:32 PM
I am unable do debug in Stm32CubeIDE 1.2.1 because I'm getting the following message:
"Failed to execute MI command". It is failing download verification:
Error: Data mismatch found at address 0x08002814 (byte = 0x7B instead of 0x1A)
If I use the ST-Link program, the target is programmed and verification passes.
2020-02-10 11:29 AM
Sure is quiet around here lately....
2020-02-11 6:53 AM
The only way I have been able to debug is to use OpenOCD. However, one thing I need to do is use the External Loader to load external flash. This is available when the Debugger is set to ST-Link, but I do not see an External Loader available when the Debugger is set to OpenOCD.
I would appreciate any ideas on how to solve this issue..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.