cancel
Showing results for 
Search instead for 
Did you mean: 

JTAG : Debuggin the memory-mapped OCTOSPI RAM or FLASH

BRado
Associate II

Hello,

It'is possible to configure Debugger to access to an external memory-mapped Memory (OCTOSPI) ?

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Andreas Bolsch
Lead II

Depends on the meaning of "debugger accesses". When it's memory mapped (and MPU doesn't interfere), it's mapped into the CPU's memory space like an internal memory, so the debugger has full *READ* access. However, write access is a different matter, so e.g. software breakpoints don't work in a straightforward way ...

BRado
Associate II

Exactly, can you explain the way to allow the write access to debugger ?

Thank's

Andreas Bolsch
Lead II

That's totally unrelated to a debugger. The OctoSPI and the external memory have to be set up properly to be accessible by the CPU in memory mapped mode, then it is accessible by a debugger, too.

In general for NOR flash: not possible, as write means: 1) erase affected (sub-) sector, 2) write. And both operations need setting the write enable by an extra command, and after erase/write polling for end of operation. For SPI-RAM (these are rather exotic) one would configure the RAM for sequential addressing mode first, then set up the write CCR, write instruction, ... registers in same fashion as the read counterparts. Then the memory-mapped mode would work for read and write in the same way (albeit much slower) as for internal RAM.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.