2025-08-05 4:15 AM
Hi all
/*
* usb_device.h
*
* Created on: Aug 5, 2025
* Author: mmadha
*/
#ifndef USB_DEVICE_H_
#define USB_DEVICE_H_
#include "usb_standards.h"
struct UsbDevice
{
/// \brief The current USB device state.
UsbDeviceState device_state;
/// \brief The current control transfer stage (for endpoint0).
UsbControlTransferStage control_transfer_stage;
/// \brief The selected USB configuration.
uint8_t configuration_value;
/** \defgroup UsbDeviceOutInBufferPointers
*@{*/
void const *ptr_out_buffer;
uint32_t out_data_size;
void const *ptr_in_buffer;
uint32_t in_data_size;
/**@}*/
};
#endif /* USB_DEVICE_H_ */
For some reason, I am getting the error Description Resource Path Location Type
expected ';', identifier or '(' before 'struct' usb_device.h /clk_test/Core/Inc line 16 C/C++ Problem
which I don't understand. Any suggestions on what could be causing this error would be greatly appreciated.
Kind regards
Solved! Go to Solution.
2025-08-05 7:24 AM
The issue is the content within the usb_standards.h file. The last statement in there, whatever it is, is missing ";". Whitespace is ignored so the error is caught on the next statement.
2025-08-05 4:27 AM
You missing a ; at the end of the usb_standards.h file.
2025-08-05 7:00 AM
isn't that a preprocessor directive, so i dont need to add a ; at the end of it
2025-08-05 7:24 AM
The issue is the content within the usb_standards.h file. The last statement in there, whatever it is, is missing ";". Whitespace is ignored so the error is caught on the next statement.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.