STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32Cube IDE getting slow compilation

Case Description: Dear All,My STM32Cube IDE taking lost of time to compile to code previously it was taking 20sec only but now it taking 10 min and compile 20% code, please suggest what the issue,CPU - I7RAM - 16 CPU Utilization - <30%RAM utilization...

vchau.2 by Associate III
  • 1781 Views
  • 6 replies
  • 1 kudos

Not able to configure Google tests with STM32Cube IDE

I have installed STM32Cube IDE and created project successfully.Generated basic programming and tried to create google test to create test cases. But while creating C/C++ Unit under C/C++ tests getting error in C/C++ application in Main tab.Attached ...

SasiSree by Associate
  • 695 Views
  • 3 replies
  • 1 kudos

SAI Function call generates unexpected data stream

Hello Board,I hope you are all having a great summer. I am currently trying to configure the 144 devolopment board with the STM32H723zg chip, to run the built in SAI peripheral. Specifically I want to transmit a frame of 256 bits, with 16 slots and s...

Kewin_J_0-1754294935646.png Kewin_J_1-1754294961236.png Kewin_J_2-1754294984806.png Kewin_J_3-1754295150919.png
Kewin_J by Associate II
  • 586 Views
  • 1 replies
  • 0 kudos

Resolved! How to produce list of pin assignments?

Hello, all,I'm using STM32CubeIDE to design my first STM32 micro-controller circuit. I've used the tool to assign functions to about 20 pins on the micro-controller so far. Now, I'm at the stage where I'm creating the schematic and connecting externa...

KevinZ by Associate III
  • 6389 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.