2020-03-18 3:04 AM
Hello, I'm trying to communicate between two STM boards through CAN. I'm using STM32F103ZET6(as Transmitter) and STM32F103C8(as Receiver). I'm not getting the output,
can I get the code? or tell me the method to debug my code in STM32IDE.
2020-03-19 8:50 AM
Мне удало�?ь �?в�?зать 2 stm32f103 на �?коро�?ти 100000 без тран�?ивера. (MBED).
I managed to connect 2 stm32f103 at a speed of 100000 without a transceiver. (MBED).
2020-03-19 9:05 AM
Perhaps start with the wiring?
See Tiny CAN method described by Keil for a simple MCU to MCU connection using diodes rather than a transceiver. CAN expects to see feedback of CAN_TX on CAN_RX to know if it successfully driving the bus or conflicting with another controller.
http://www.keil.com/appnotes/files/apnt_236_v2.9.pdf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.