2024-04-01 7:28 AM - edited 2024-04-02 1:15 AM
I'm using STM32CubeIDE (Linux generic version) on Linux Mint Debian Edition, KDE Window Manager.
When starting it as normal user the Themin is not working (Preferences-General-Appearance). The window has a dark theme (the one I choose in my KDE preferences). But I would like to use the default light theme.
The only way to do this is by running STM32CubeIDE with sudo. Is this expected or is there a workaround?
Thanks
Solved! Go to Solution.
2024-04-02 1:22 AM
I found the solution for this. You have to add a line to the startup script "stm32cubeide_wayland" which is located in the stm32cubeide_x.xx.x folder
Before the last line that starts cubeide add the line:
export GTK_THEME=Adwaita
Would be nice if this could be added by ST per default into this script.
2024-04-02 1:22 AM
I found the solution for this. You have to add a line to the startup script "stm32cubeide_wayland" which is located in the stm32cubeide_x.xx.x folder
Before the last line that starts cubeide add the line:
export GTK_THEME=Adwaita
Would be nice if this could be added by ST per default into this script.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.