2024-11-07 11:55 PM
Hi all,
basic info:
stm32 CUBE IDE v1.14.1
PC: Win10 64bit
MCU:STM32G0B1CC
In my code, there are two functions to control the battery to enter charge mode from init mode, when the battery receive a command. Check_AuthCmdToCHG()will set CANOpenStruct.flag_authCmdGotoCHG to STD_TRUE and set CANOpenStruct.sendTPDOInfo STD_TRUE.
normally,after CANOpenStruct.flag_authCmdGotoCHG be set to STD_TRUE , CheckFlag_InitGotoCHG() will make state machine FSM goes to charge mode.
But it's very strange, i send a command to MCU, then I receive TPDO info from CAN bus, this means CANOpenStruct.sendTPDOInfo already be set to STD_TRUE. however CANOpenStruct.flag_authCmdGotoCHG and CheckFlag_InitGotoCHG() are not work!
When I examined the code, I couldn't find the cause. Therefore, I wrote a test function Test_CANCmd() ready to read CANOpenStruct.flag_authCmdGotoCHG and CANOpenStruct.sendTPDOInfo out, the other did not modify any code! I compile the code and burn it like before. Then something amazing happened. Everything worked!
is there anyone can explain this? The Test_CANCmd()function just uses the value of CANOpenStruct.flag_authCmdGotoCHG, FSMStruct.flag_initGotoCHG and does not change it, why does it have such an effect?
void Check_AuthCmdToCHG(void)
{
if(sysInfoStruct.statusCharger == STD_FALSE)
{
if(pinStatus_present == STD_ON)
{
if(sysInfoStruct.chargerOnline == 0x1234)
{
sysInfoStruct.statusCharger = STD_TRUE;
CANOpenStruct.flag_authCmdGotoCHG = STD_TRUE;
CANOpenStruct.sendTPDOInfo= STD_TRUE; //if true,it will enable CAN TPDO
}
}
else
{
sysInfoStruct.chargerOnline = 0;
}
}
}void CheckFlag_InitGotoCHG(void)
{
if(pinStatus_present == STD_ON)
{
if(CANOpenStruct.flag_authCmdGotoCHG == STD_TRUE)
{
CANOpenStruct.flag_authCmdGotoCHG = STD_FALSE;
FSMStruct.flag_initGotoCHG = STD_TRUE;
}
}
}uint32 Test_CANCmd(union_64bits cmd)
{
//..........
switch(cmd.byte[2])
{
case 0xF1:
//......
break;
case 0xF5: //ESD Pres pin onoff times test
if(cmd.byte[3] == 0xFF)
{
errCode = CANOpenStruct.flag_authCmdGotoCHG;
}
else if(cmd.byte[3] == 0xFE)
{
errCode = FSMStruct.flag_initGotoCHG;
}
else
{
errCode = TEC_cmdParaErr;
}
break;
//..........
}
return errCode;
}
Solved! Go to Solution.
2024-11-17 11:53 PM
My problem has been solved!
Root cause: STM32G0B1CC is based on Arm Cortex -M0+ core, it no support unaligned accesses, pay attention to the large structure in your code.
2024-11-08 12:19 AM
If you have debugging enabled, print the values of flag_authCmdGotoCHG, sendTPDOInfo, and FSMStruct.flag_initGotoCHG right after setting and reading them to observe any anomalies.
2024-11-10 4:58 PM
Hi liaifat85,
Thanks for your feedback!
My current APP code is address offset because the system comes with a bootloader. I have tried to modify the offset address and directly run online simulation, and the program works normally.
I have tried the following 2 situations:
S1:
Comment out the code for CANOpenStruct.flag_authCmdGotoCHG and FSMStruct.flag_initGotoCHG , without changing anything else, and the program works abnormally.
uint32 Test_CANCmd(union_64bits cmd)
{
//..........
switch(cmd.byte[2])
{
case 0xF1:
//......
break;
case 0xF5: //ESD Pres pin onoff times test
/*
if(cmd.byte[3] == 0xFF)
{
errCode = CANOpenStruct.flag_authCmdGotoCHG;
}
else if(cmd.byte[3] == 0xFE)
{
errCode = FSMStruct.flag_initGotoCHG;
}
else
{
errCode = TEC_cmdParaErr;
}
*/
break;
//..........
}
return errCode;
}S2:
Keep CANOpenStruct.flag_authCmdGotoCHG and FSMStruct.flag_initGotoCHG code, do not change other codes, the program works fine.
2024-11-17 11:53 PM
My problem has been solved!
Root cause: STM32G0B1CC is based on Arm Cortex -M0+ core, it no support unaligned accesses, pay attention to the large structure in your code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.