2024-02-18 7:43 AM
Basically what I said in the title. After rebuilding and running, it first runs the most recent previous build and then after a few seconds, the newest build.
I even made a new project from scratch but I get the same result.
I am using an STM32F411RE. I only autogenerated the code for USART2 and it's global interrupt. I then added 2 lines of code to transmit a string to Termite. I never use the global interrupt.
My added code:
uint8_t stdnum[] = "&_25962906_*\n" ;
HAL_UART_Transmit(&huart2, stdnum, strlen((char*)stdnum), HAL_MAX_DELAY);
2024-02-18 12:48 PM - edited 2024-02-18 12:48 PM
What do you mean by it runs the previous build? How does the previous build differ from the current build? If you've modified a file, the previous version of that file no longer exists on disk, at least not in a manner than STM32CubeIDE can access.
Perhaps some screenshots would help. It could be you're misinterpreting another project being built, or another action taking place.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.