2023-10-19 9:51 PM
I would like to use 2 Compiler in one project, the old compiler for the bootloader, where addresses should not change for application and the other for the application to use a newer version.
First I tried to select either or from the C/C++ Build -> settings -> MCU Toolchain -> Fixed where I can select GNU Tools for STM32... or my own installed GNU, which I added in the Toolchain Manager.
But the IDE always uses the compiler which folder is listed first in PATH.
Final target is to select the compiler based on folders.
is there a possiblity?
2023-10-27 8:31 AM
Hello @koster
First let me thank you for posting.
To be able to use two different toolchains for the same project, you need to set a different toolchain for each debug configuration.
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.