2019-10-10 1:33 AM
I have just reinstalled CubeIDE on a new PC and trying to work on some already created project with CubeIDE.
The target is an STM32F7.
I opened the Cube .ioc file from inside CubeIDE explorer, then modify some settings.
When I try to save, I get a message saying that stm32cube is being updated.
Then imediately after a message saying "Error downloading the following files: stm32cube_fw_f7_v1150.zip (Not available).
Then all the files in my project get permanently deleted leaving only the .project and the .ioc file!
And when I say permanently, I do mean it is not in the bin!!!
This is the second time it happened to me in a week.
And the second time I loose one day worth of work.
2019-10-13 5:52 AM
After a lot of trial and errors, I finaly find the root!
The workspace I am working on was created on another computer which had STM32CubeIDE v1.0.0 aswell as STM32CubeMX installed separately.
Now I am working on a different computer which has STM32CubeIDE v1.0.2 and no STM32CubeMx.
I am not sure which one is relevant here: the version or the fact that STM32CubeMx is present on the first computer.
Anyway, in the file .metadata\.plugins\org.eclipse.core.runtime\.settings\com.st.stm32cube.common.mx.prefs which was created with the first computer, the following entry is present: STM32CubeMX.FirmwareRepositoryPath=C\:/Users/Franck/STM32Cube/Repository/
Removing this entry from the workspace fixes the issue.
This entry is not present if I create a workspace with the second computer (again not sure if it is link to STM32CubeIDE v1.0.2 or no STM32CubeMx)
However, it is exported with the eclipse preferences (file->Export->General->Preferences), so if I create a new workspace and import my old preferences, I get the same issue.
I do hope that ST will fixe this bug.
I understand that this is a particular case and it won't affect a lot of people, but the the fact that all source files in a project could be permanetly erased without warning is quite alarming.
2019-10-15 11:48 AM
Sounds lacking firmware packs at a time may have lead to such behavior pain. Definitively a bug.
Sounds some improvements have been done fixing such issue Thanks STM32CubeIDE V1.1.0 just released on st.com
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.