STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Is the HAL IRQ callback function running outside of irq context ? Is this a good place for some string processing ?

I am currently working with UART in DMA mode for CLI implimentation. I would like to do some string parsing as part of the HAL_UART_RxCpltCallback.Is this callback running in IRQ context or outside of IRQ context ? Is this the correct place for post...

PRedd.5 by Associate II
  • 2529 Views
  • 4 replies
  • 0 kudos

Hardfault error Float

Hi,I am using stm32 f407 for my project. I have set stack size min 0x6000. I am using STM Cube IDE. In one of the project files I have a float assignmentfloat val = resizedImage[i]; I have enabled FPU in the systemInit() function. I have set FPU_P...

SPrak.4 by Associate II
  • 2525 Views
  • 2 replies
  • 0 kudos

Live Expression refresh rate and Semihosting

I have two questions about the IDE:Is there a way to change the refresh rate of the variables in Live Expressions?Semihosting works only with OpenOCD. The problem with OpenOCD is that the Live Expressions doesn't work. Are you going to implement the ...

JHilj by Associate
  • 1109 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.