2025-04-23 10:58 PM
I am using STM32CubeIDE to program my board i.e. STM32H7S78-DK. My file size is in large due to which it is flashing in external flash at address 0x70000000. In case of smaller file size i.e. less than 64 KB, it flashes in internal flash at address 0x08000000. The flashing was working fine in internal as well as external flash. But, all of a sudden, I am getting below error log.
-------------------------------------------------
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: C:\Users\<Username>\AppData\Local\Temp\STM32CubeProgrammer_a40504.log
ST-LINK SN : 0046001A3033511935393935
ST-LINK FW : V3J16M7
Board : STM32H7S78-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x485
Revision ID : Rev Y
Device name : STM32H7RSxx
Flash size : 64 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0xE3
Opening and parsing file: ST-LINK_GDB_server_a40504.srec
Memory Programming ...
File : ST-LINK_GDB_server_a40504.srec
Size : 53.59 MB
Address : 0x70000000
Erasing memory corresponding to sector 0:
Erasing external memory sectors [0 7]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
-----------------------------------
Screenshot attached. Kindly help me with this issue.
2025-04-25 11:19 AM
I just ran into a similar problem myself.
I was able to get external flash erasing to work again using the following procedure.
I hope this helps!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.