2024-08-28 6:24 AM
Hi,
I have been trying to place a function in the ITCM region for some time with no luck. As close I get was HardFalult There are some examples for the F7 series on the web. Some dating back to 2016, some similar to F767 with the same core but I cannot make them work. Each example uses a different way, making it harder to figure out. Modifying the linker file, modifying the startup.s file.
Yes, I read AN4667.
I am using STM32CubeIDE 1.1.16.
Is there a clear application note or up to date example code that I can use?
Best regards,
Tim
Solved! Go to Solution.
2024-08-29 7:58 AM
Hello,
Maybe you can check this article it can help you: How to place and execute STM32 code in SRAM memory with STM32CubeIDE.
2024-08-29 7:58 AM
Hello,
Maybe you can check this article it can help you: How to place and execute STM32 code in SRAM memory with STM32CubeIDE.
2024-09-01 10:28 PM
Hi,
I can run from RAM without a problem but not from ITCM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.