2023-12-26 5:21 PM
In STM32F746G Discovery board product Speifications, it is shown as
But it has not given whether STM32CubeIDE works with it or not.
Need clarification on this.
2023-12-26 7:46 PM
Hello @Moni and welcome to the ST Community :smiling_face_with_smiling_eyes:.
The STM32CubeIDE is a GCC-based IDE. So, it is supported by the STM32F746G Discovery board.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.