2024-02-08 7:09 PM
Hi,
I use the STM32F429I-DISC1 board with STM32CubeIDE 1.7.0.
I can compile the project.
But I upgraded the IDE to Rev 1.14.1.
I cannot compile the project. It occurred a lot of error.
What are different between STM32CubeIDE Rev 1.7.0 and Rev 1.14.1?
Must I setup something before using STM32CubeIDE Rev 1.14.1?
Thank you
Solved! Go to Solution.
2024-02-09 12:08 PM - edited 2024-02-09 12:11 PM
The main relevant change is a newer default toolchain (compiler etc.). Install the same toolchain that you've used in the previous CubeIDE version, and set is as the toolchain for your project. Settings-> MCU Toolchain. Enjoy.
2024-02-08 7:39 PM
What are the errors? Start with the first one shown in the output window, solve it, progress from there.
2024-02-09 12:08 PM - edited 2024-02-09 12:11 PM
The main relevant change is a newer default toolchain (compiler etc.). Install the same toolchain that you've used in the previous CubeIDE version, and set is as the toolchain for your project. Settings-> MCU Toolchain. Enjoy.
2024-02-12 2:19 AM
Hi Pavel A,
I found the issue of MCU Toolchain revision.
- The MCU Toolchain of STM32CubeIDE 1.7.0 is GNU Tools for STM32 (9-2020-q2-update).
- The MCU Toolchain of STM32CubeIDE 1.14.1 is GNU Tools for STM32 (11.3.rel1).
I downloaded the GNU Tools for STM32 (9-2020-q2-update) and set to default.
I can compile the project successfully.
Thank you very much for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.