2026-01-12 7:07 AM
Hello. I am currently working on a NUCLEO-L152RE project in the latest version of the CubeIDE. I am running into an error where I can not install break points due to an "unmatched quote". I have tried the common fixes (New work space) for this that I could find online and it hasn't resolved it. I also ran fresh installs of the programs and encountered the same issue. Has anyone else encountered this problem? I have included a screenshot below for reference.
Solved! Go to Solution.
2026-01-12 8:38 AM
@ddwertz wrote:This is the file path shown in the IDE
I added a PS to my previous post - it looks like the single quote might also upset things...
Check also what "OneDrive - Personal" actually translates to ...
2026-01-12 7:21 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results
In particular, what version of Cube are you using, and on what platform?
Please describe in detail the steps you take to get to this error.
@ddwertz wrote:I am currently working on a NUCLEO-L152RE project
Is this a project you've created yourself, an ST example, or something else?
2026-01-12 7:22 AM
Does the project build and run successfully?
Maybe there is an unmatched quote in the file or a file it includes. It's unlikely to be making things up--this is parsed, not AI.
2026-01-12 7:34 AM
I am using the 2.0.0 Build of both the IDE and MX software. I used the MX file to generate the initial code and then added some generic lines (incrementing an integer). This is the second project I have created using the MX and they both have the same problem. I am running the software on a Windows 11 set up. As far as I can tell everything functions properly except for the breakpoints.
2026-01-12 7:38 AM
The project builds and runs as intended. The breakpoint is to be inserted as part of a lab exercise to show functionality. When I manually stop/start the program it functions as intended, it just won't allow me to insert a breakpoint. As far as the included files I generated it in MX (ver 2.0.0).
2026-01-12 7:45 AM - edited 2026-01-12 7:47 AM
Please give detailed steps of what you're doing to get this message.
PS:
@ddwertz wrote:part of a lab exercise .
So have you shown this behaviour to your lab supervisor?
2026-01-12 8:00 AM
I have shown it to the TA and he was unfamiliar with it, ended up using the older version of the IDE (1.9.0 I think) to run the labs last week to complete it. I have spoke with the course instructor and he was unsure as well. I reached out to the course instructor over email last Wednesday after performing fresh installs and haven't heard back yet. I am going to the TA office hours today to get more assistance.
As far as specific steps, I generated the initial file in the MX (ver 2.0.0). I then opened the project in my CubeIDE workspace (ver 2.0.0). Then I added two lines. The first declared the variable myInt and set the value to 0 "uint8_t myInt = 0;". The second increments myInt in the generated while loop "myInt++;". I only get an error when I add the breakpoint to any of the lines in the main.c file, using both the add breakpoint option and double clicking the line number.
Adding the breakpoints generates the message, I am getting no other warnings or errors. It has effected every .c file in multiple projects that I have worked on.
2026-01-12 8:24 AM - edited 2026-01-12 8:34 AM
@ddwertz wrote:MX (ver 2.0.0). .
The latest version is 6.16.1 (there's been an update since this announcement).
So, after adding your lines, you build the code, and then start the debugger - yes?
Then, once you're in the Debug Perspective, you set the breakpoint ?
Are there any spaces or other "special" characters in any of your file or folder names?
PS:
Just found this, reporting the same issue in another Eclipse-based IDE, where spaces in the path were, indeed, the problem.
Spaces and other "special" characters are an all-too-common source of grief and weird behaviour - see here.
2026-01-12 8:31 AM
You're correct in the file version. I mis-listed what I have for it. I downloaded the latest from last Wednesday.
Yes, in the Debug perspective I set the breakpoint after adding/building the files.
This is the file path shown in the IDE
This is the file path as shown in the explorer.
I will remove the spaces in the file names and see if that fixes it.
2026-01-12 8:38 AM
@ddwertz wrote:This is the file path shown in the IDE
I added a PS to my previous post - it looks like the single quote might also upset things...
Check also what "OneDrive - Personal" actually translates to ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.