2024-03-19 4:03 PM
Hi all,
I have a STM32C011 project. I am using a STMF0-Discovery as a ST-Link, as I have done many times before.
I have upgraded STM32CubeIDE to V1.15. It is asking me to upgrade the firmware in the ST-Link. Going through the upgrade process, it fails stating "Unexpected flash size for ST-Link micro. Don't know how to upgrade".
If I select No to the upgrade request, CubeIDE stops there...
I used STM32CubeProgrammer to upgrade the firmware in the ST-LInk, and STM32CubeProgrammer is happy to work with it.
But STM32CubeIDE V1.15 won't work with it!
How do I get it to work?
Thanking you
Pedro
2024-03-19 4:20 PM
> I am using a STMF0-Discovery as a ST-Link
Do yourself a favor: get a new ST-LINKv3.
2024-03-19 5:08 PM
Thanks for your reply.
However, the STMF0-Discovery has multiple functions in this project.
Adding another module is not the solution I'm looking for.
Kind regards
Pedro
2024-03-19 8:09 PM
Then disable ST-Link version checking in CubeIDE to be able to debug the F0 board. (And get a ST-Linkv3 for the STM32C0)
2024-03-19 10:03 PM
@Pavel A. wrote:Then disable ST-Link version checking in CubeIDE to be able to debug the F0 board. (And get a ST-Linkv3 for the STM32C0)
Thank you for your reply, however, I clearly said -
If I select No to the upgrade request, CubeIDE stops there...
and
However, the STMF0-Discovery has multiple functions in this project.
Adding another module is not the solution I'm looking for.
Kind regards
Pedro
2024-03-20 12:22 AM
I have been having the same issues; since then a lot of my programs can't flash onto the board and the behaviour of the ST-LINK is very weird. When I open up a program on debugger during the rare-times it does work there is no uart output and some programs when I flash fail
2024-03-21 8:23 PM
It seems V1.15 has more problems, i was working on a project the upgrade was ready i closed the project and did the upgrade. Then went back to my project. Now i cannot download my code for debugging, getting some very odd error message. Screen shot attached. I can still connect to the hardware using STM32CubeProgrammer no problem.
i would also suggest getting a STLINKV3. My old STLINKV2 will not upgrade under V1.15.
i was hoping some of the bugs and instabilities in the IDE would have been fixed now i cannot do my work. this i caused by upgrading.
2024-03-21 9:06 PM
Seems there is a regression somewhere with V1.15
See https://community.st.com/t5/stm32cubeide-mcus/problem-after-updating-cubeide-to-1-15-0/td-p/653175
and
2024-03-21 11:16 PM
Hello,
Try this workaround to unblock your situation until this issue get fixed in CubeIDE
2024-03-24 8:28 PM
Hi,
I have tried the above workaround. Unfortunately it does NOT work! I get
Verifying... ################################# [100%]
Preparing... ################################# [100%]
package st-stlink-udev-rules-1.0.3-2.x86_64 is already installed
and the problem persists...
Kind regards
Pedro
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.