2026-02-21 10:41 AM
Hello, I installed STM32CubeIDE and attempted to set up my first project as you can see in the three attachments.
Based on YouTube videos, I expected to see the MCU outline so I can assign functions to the pins. As you can see in one of the screenshots, I'm getting a message stating that "There is no active editor that provides an outline"
I did the following to try and address this, with no luck...
* Uninstalled and Reinstalled STM32CubeIDE, including manually deleting folders that were not removed by the automated removal process. To be safe, I used a different project folder name but this didn't help.
* Installed STM32 on a second Windows 11 laptop but saw the exact same problem
I didn't bother trying older versions of STM32CubeIDE because I read in a different post that this did not solve the problem for the other user.
Any help is appreciated.
Solved! Go to Solution.
2026-02-21 10:55 AM
Use standalone STM32CubeMX to generate a project. You can't do so in STM32CubeIDE anymore.
STM32CubeIDE 2.0.0 released - STMicroelectronics Community
STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community
2026-02-21 10:55 AM
Use standalone STM32CubeMX to generate a project. You can't do so in STM32CubeIDE anymore.
STM32CubeIDE 2.0.0 released - STMicroelectronics Community
STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community
2026-02-21 11:08 AM
Thanks TDK!!!
2026-02-21 11:11 AM
If you have any sway with the ST SW dev folks, I suggest that they improve the error messages that are displayed when someone makes this mistake.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.