2020-12-16 2:59 AM
Hi all,
I am testing H745 processor on Nucleo-H745ZI-Q board and STM32CubeIDE 1.5.0 .
I started from a demo project found in Cube library, which handles both CM7 and CM4 cores.
The IDE correctly creates one HEX file for CM4 and another HEX file for CM7, then creates a single HEX file which hopefully contains both.
It is not clear to me where are the project config options which are creating the final HEX file (CM4+CM7) : is there someone who can give me a hint for this ?
The IDE is working correctly, but I am not so "comfortable" in missing these configs.
Thanks,
regards && best wishes for Christmas and new year to all !
Lucio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.