2026-05-01 6:42 AM
In STM32CubeIDE 2.1.1, Project Explorer keeps collapsing constantly.
This has been a persistent bug for a very long time and is very annoying.
Can't ST just fix this since it is based on Eclipse?
2026-05-04 2:56 AM
Hello @Jack3
The recommended solution is to create a new STM32CubeIDE workspace, because this is the safest and most effective way to remove corrupted UI or metadata state without touching the actual project files.
Go to File → Switch Workspace ,select a new empty workspace from this menu, restart STM32CubeIDE in that fresh workspace, and then re-import the existing project.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.