2022-03-28 8:56 AM
Hi Community,
The env is: STM32CubeIDE 1.8.0, macOS 10.15.7, MBP16-2019
When STM32CubeIDE is running, the OS switches to discrete GPU and eat about 30W totally(with integreted GPU only 10W is needed). The battery is running low fast.
I force switch to integreted GPU with gSwitch. Everything seems OK.
So would ST please check why STM32CubeIDE is designed to depends on discrete GPU on macOS? If it is not necessary, it would brings huge convenince to remove the dependency.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.