2025-01-16 4:04 AM
Hello, I'm having an issue with the STM32CubeIDE configuration.
Due to company policy, my development PC does not have internet access, so I need to set up STM32CubeIDE offline.
So, even though I installed the relevant STM32Cube for G0 series, I’m getting a “missing dependencies” error.
Why is it happening? What else do I need to install to resolve this issue?
Also, is there a way to check which dependencies are missing?
Thank you in advance.
2025-01-16 4:22 AM
Hello @Sungjae Kim ,
To install the package offline, please follow the steps in this article:
2025-01-17 2:39 PM
Hello @Imen.D ,
I followed the instructions from that link, but there wasn’t much progress.
Here are the results I found after further investigation:
If I only download and install version 1.X.0 (without applying any patches), then create a new project using the MCU selector while choosing 1.X.0 as the Cube version, the project is created successfully.
If I apply a patch, the problem persists even when selecting the correct version (in some series the patch applies properly, but usually the issue occurs).
Even with only version 1.X.0 installed, if I create a project through the Board selector, the problem can occur as well (depending on the board).
2025-01-20 12:30 PM
Hi All,
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Jake
ST Support
2025-06-12 12:14 AM
i have the same problem i cannot download the patch when my pc is offline is there an update on this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.