2023-10-06 1:22 PM
After having a problem with the generic Linux installation I uninstalled STM32CubeIDE and instead installed the Debian version. It loads up but when I click on File>New STM32 Project it says STM32 target or STM32CubeIDE example selection is required. Can't progress past that point. Log file attached
2023-10-19 6:40 AM - edited 2023-10-19 6:41 AM
Hello @Dabbo,
Thank you for posting.
Can you share the .log file and provide a screenshot of the STM32CubeIDE issue.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.