2020-05-14 2:29 AM
Hello,
I noticed that when I want to copy a project into the same workspace, the following issues occur:
Yesterday I upgraded to version 1.3.1 build 6291_20200406_0752 (UTC), but I see that these issues are not been corrected.
s.
2020-05-14 3:43 AM
We are aware of issues when both copying and (for example) renaming projects. It's on our list of fixes we want to do.
2020-06-10 9:18 PM
I have been working around this issue by manually renaming the .ioc file with the new project name.
Then manually delete previously generated /Debug and /Release directories and debug launch files.
I then manually refresh the project and rebuild the index as a precaution.
After that you can select the .ioc file to launch mx cube within the project.
WARNING. I do not recommend doing this though. I think that the first time the renamed .ioc file is used in the new project, it deletes the /Core/Src directory of the previous project. But the renamed .ioc file operates as expected in the new project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.