STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32Cube IDE issues

If you delete the project folder from the workspace and then put there a copy previously made from the archive, the Cube will not be able to open it.How can I solve this issue?

olezhandr by Associate III
  • 1009 Views
  • 1 replies
  • 1 kudos

Partial error with custom external loader

Hello,i created my own external loader for STM32F767IGT MCU with W25Q256 QuadSPI FLASH.When i read its memory with STM32CubeIDE i can see all of it and the test works perfectly. But when i read it with STM32 Programmer i see only 99999999 until about...

0693W000001qN8GQAU.png
AMerc.4 by Senior
  • 751 Views
  • 0 replies
  • 0 kudos

compilation STMCubeIDE nosys.spec

Upon building with STM32CubeIDE I just get > collect2: error: ld returned 1 exit status> make: *** [makefile:44: help.elf] Error 1Calling arm-none-eabi-gcc directly gets me> arm-none-eabi-gcc: error: nosys.specs: No such file or directoryAny suggesti...

SWink by Associate II
  • 2777 Views
  • 4 replies
  • 0 kudos

Im trying to get LWIP to connect to a remote server, but im returned with Routing error ( err_t ERR_RTE) when calling tcp_connect(). The card is a Nucleo F746ZG and im using stm32QubeIDE with LwIP added as a middleware

Snuippet of source code /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART3_UART_Init(); Print("USART init ok\n"); MX_USB_OTG_FS_PCD_Init(); Print("USB pcd init ok\n"); MX_LWIP_Init(); Print("LWIP init ok\n"); /* USER CODE BEGIN 2 -...

DIsak.1 by Associate
  • 1068 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.