2019-05-07 7:24 AM
Title says it all. I cannot create a new project - the model dialog for 'select STM32 target' is blank.
Freshly installed the from .deb_bundle.sh installer without errors.
Running Ubuntu 19.04 with vanilla gnome-session installed.
2019-10-10 2:15 AM
Worked for me as well, thanks !
2020-02-25 3:08 PM
If you normally open the IDE using the search bar or a shortcut icon, you can always have this fix by editing the associated .desktop file for the STM32CubeIDE shortcut:
sudo emacs /usr/share/applications/st-stm32cubeide-1.3.0.desktop
Change:
Exec=/opt/st/stm32cubeide_1.3.0/stm32cubeide %F
To:
Exec=/usr/bin/env GDK_BACKEND=x11 /opt/st/stm32cubeide_1.3.0/stm32cubeide %F
2020-05-16 9:00 PM
I was able to sort this out on my Fedora 32 install by adding a line to my /usr/share/applications/st-stm32cubeide-1.3.0.desktop file.
Much like GBeck.1's answer, I simply added the line...
Exec=/usr/bin/env GDK_BACKEND=x11 export GDK_BACKEND
above the existing Exec line in the aforementioned .desktop file so that it (in total) looks like this ...
[Desktop Entry]
Name=STMicroelectronics STM32CubeIDE 1.3.0
Comment=STMicroelectronics STM32CubeIDE 1.3.0
GenericName=STM32CubeIDE
Exec=/usr/bin/env GDK_BACKEND=x11 export GDK_BACKEND
Exec=/opt/st/stm32cubeide_1.3.0/stm32cubeide %F
Icon=/opt/st/stm32cubeide_1.3.0/icon.xpm
Path=/opt/st/stm32cubeide_1.3.0/
Terminal=false
StartupNotify=true
Type=Application
Categories=Development
I now get the target page populated and I can continue on.
2020-05-23 11:20 PM
I am still having this problem on Ubuntu. I have downloaded the debian version of stm32cubeide, and when I open it and select start new stm32 project it brings up the target select screen but it is completely blank and the only valid option is "cancel." I have tried running:
$GDK_BACKEND=x11
$export GDK_BACKEND
$/opt/st/stm32cubeide_1.3.0/stm32cubeidebut this didn't work. I have also tried adding Exec=/usr/bin/env GDK_BACKEND=x11 export GDK_BACKEND as GeoFoz suggested and changing the line to Exec=/usr/bin/env GDK_BACKEND=x11 /opt/st/stm32cubeide_1.3.0/stm32cubeide %F as GBeck.1 suggested. But I am still seeing the same thing. I have also tried rebooting the computer and uninstalling & reinstalling the software.
Is there any thing I am missing? Does x11 need to be installed / how would I do that? (google doesn't have a clear answer, I thought x11 was default in ubuntu)
2021-04-23 1:12 AM
Thank you so much! still works on ubuntu 21.04!
2021-06-28 1:56 AM
This did it for me, thank you very much! I am using Debian Buster 64 bit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.