2025-11-18 8:06 AM
Hello,
I tested the new STM32CubeIDE 2.0 today and was initially confused that CubeMX opened when I double-clicked on the *.ioc file. However, this is listed as a new feature in the release notes.
Unfortunately, this feature completely destroys my projects.
When the code is generated, these settings in the CubeIDE project change:
- Targeted Language changes from C++ to C
- Linked folders are deleted
- Configurations: DEBUG, SYSTEM added
- Linker file settings from own configurations deleted
Did I make a mistake in the settings? Why is the project changed so much?
Best regards,
Jens
Solved! Go to Solution.
2025-11-20 7:58 AM
Hello @JensH ,
The issue is confirmed: Restoring previously the deleted DEBUG/RELEASE configurations on STM32CubeIDE 2.0
and reported to the dedicated to the Dedicated Team.
Your contribution and interaction are greatly appreciated.
Best Regards.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-20 8:38 AM
Hello Jens,
This isn’t a mistake on your side. In STM32CubeIDE 2.0, opening the *.ioc file automatically with CubeMX can overwrite project settings—switching C++ to C, deleting linked folders, adding new configurations, and removing custom linker files.
For now, the safest approach is either to avoid regenerating code from the .ioc file or use the standalone CubeMX. Many users have reported the same issue, so it seems to be a change in 2.0 rather than a misconfiguration.
2025-11-24 5:55 AM
Hello @JensH @Theodore-henry6 @jd5 @MGogr.1
The issue is confirmed: [Linked Folders are deleted] and reported to the dedicated to the Dedicated Team.
I will let you know when the issue is fixed.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-24 7:09 AM
Hallo @Mahmoud Ben Romdhane ,
so am I right that everything I reported is confirmed and reported?
Best regards,
Jens
2025-12-01 9:28 PM
Can you make it like the previous version where we dont have to open.ioc file in MX Cube.
That will be really helpful.
2025-12-09 1:06 PM
another STM MCU FU! This is not a fix. Don't they test even the basic functions before releasing updated FGS!
2025-12-17 6:11 AM
There should really be an update in every type of documentation for this. I was just following the tutorial and the video from 5 years ago showed features I couldn't find. Including this rabbit hole I dove in to when I couldn't create a project with the graphical user interface in the IDE. Only to read the release notes for 2.0 afterward. Very frustrating!
2025-12-17 8:14 AM
While I agree it's bad that the documentation is out-of-date - especially with such a significant change - I don't think you can really complain about a 5 year old video not reflecting the latest version!
That's even older than v1.07.0 !
See this post for an up-to-date tutorial.
2025-12-17 10:24 AM
And I will totally agree with that. But then why do they have links to 5 year old videos in their documentation?
I'm not sure how I got to the video this afternoon but I think it was through the videos for tutorials directly in CubeIDE.
2025-12-17 10:31 AM
@Teun888 wrote:why do they have links to 5 year old videos in their documentation?
That's a good question!
It should, at least, be clearly flagged that it relates to a (very) old version ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.