2025-10-04 9:06 AM - last edited on 2025-10-04 9:21 AM by Andrew Neil
Hi there,
So I'm using STM32CubeIDE as is the program we use in Embedded Systems subject at my university. I installed it on Arch with GNOME 49 Wayland (I know, they hate each other) and I'm passing the GDK_BACKEND=x11 environment variable. I've already fixed the debugger not having the proper libncurses version and now I can upload code to the board but I cant visualize IOC files, board selector, etc. Any help would be very appreciated.
Thanks in advance!
2025-10-06 12:48 AM
Hello @SMT4497
Unfortunately, STM32CubeIDE is not supported on the GNOME 49 yet. Below are the supported operating systems and architectures for STM32CubeIDE
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 41
• macOS® 14 (Sonoma), macOS® 15 (Sequoia)
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.