cancel
Showing results for 
Search instead for 
Did you mean: 

ST32F469I AU1 Serial port issue on Cube IDE

Chris1001Z
Associate

Hi All 

I am having difficulty getting the serial to work through the STlink on the STM32F469I AU1 (MB1189B) version. 

I have tried all the suggestions in the previous posts on the forms. The uart is set with the correct pins according to the schematic of the MB1189B (Uart3 PB10, PB11). I have tried numerous serial monitors all settings were correct and still nothing. Is there something different in the configuration of this version of the PCB that I am missing?  I am really at a loss as to why this isn't working any suggestions Would be appreciated.

 

Also, find attached Code below were i try every port on the PCB. 

main.c

 

/* USER CODE BEGIN PV */

uint8_t tx_buffer1[10] = "UART1!!\n\r";

uint8_t tx_buffer2[10] = "UART2!!\n\r";

uint8_t tx_buffer3[10] = "UART3!!\n\r";

uint8_t tx_buffer4[10] = "UART4!!\n\r";

uint8_t tx_buffer5[10] = "UART5!!\n\r";

uint8_t tx_buffer6[10] = "UART6!!\n\r";

/* USER CODE END PV */

 

int main(void)

{

 

  /* USER CODE BEGIN 1 */

 

  HAL_UART_Transmit(&huart1, tx_buffer1, 10, HAL_MAX_DELAY);

  HAL_UART_Transmit(&huart2, tx_buffer2, 10, HAL_MAX_DELAY);

  HAL_UART_Transmit(&huart3, tx_buffer3, 10, HAL_MAX_DELAY);

  HAL_UART_Transmit(&huart4, tx_buffer4, 10, HAL_MAX_DELAY);

  HAL_UART_Transmit(&huart5, tx_buffer5, 10, HAL_MAX_DELAY);

  HAL_UART_Transmit(&huart6, tx_buffer6, 10, HAL_MAX_DELAY);

 

/* USER CODE END 1 */

 

  /* MCU Configuration--------------------------------------------------------*/

 

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

 

  /* USER CODE BEGIN Init */

 

  /* USER CODE END Init */

 

  /* Configure the system clock */

  SystemClock_Config();

 

  /* USER CODE BEGIN SysInit */

 

  /* USER CODE END SysInit */

 

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_CRC_Init();

  MX_DMA2D_Init();

  MX_DSIHOST_DSI_Init();

  MX_FMC_Init();

  MX_LTDC_Init();

  MX_QUADSPI_Init();

  MX_I2C1_Init();

  MX_USART2_UART_Init();

  MX_UART4_Init();

  MX_UART5_Init();

  MX_USART1_UART_Init();

  MX_USART3_UART_Init();

  MX_USART6_UART_Init();

  MX_TouchGFX_Init();

  /* Call PreOsInit function */

  MX_TouchGFX_PreOSInit();

  /* USER CODE BEGIN 2 */

 

  /* USER CODE END 2 */

 

  /* Init scheduler */

  osKernelInitialize();

 

  /* USER CODE BEGIN RTOS_MUTEX */

  /* add mutexes, ... */

  /* USER CODE END RTOS_MUTEX */

 

  /* USER CODE BEGIN RTOS_SEMAPHORES */

  /* add semaphores, ... */

  /* USER CODE END RTOS_SEMAPHORES */

 

  /* USER CODE BEGIN RTOS_TIMERS */

  /* start timers, add new ones, ... */

  /* USER CODE END RTOS_TIMERS */

 

  /* USER CODE BEGIN RTOS_QUEUES */

  /* add queues, ... */

  /* USER CODE END RTOS_QUEUES */

 

  /* Create the thread(s) */

  /* creation of defaultTask */

  defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);

 

  /* creation of TouchGFXTask */

  TouchGFXTaskHandle = osThreadNew(TouchGFX_Task, NULL, &TouchGFXTask_attributes);

 

  /* USER CODE BEGIN RTOS_THREADS */

  /* add threads, ... */

  /* USER CODE END RTOS_THREADS */

 

  /* USER CODE BEGIN RTOS_EVENTS */

  /* add events, ... */

  /* USER CODE END RTOS_EVENTS */

 

  /* Start scheduler */

  osKernelStart();

 

  /* We should never get here as control is now taken by the scheduler */

 

  /* Infinite loop */

  /* USER CODE BEGIN WHILE */

  while (1)

  {

  HAL_Delay(1000); // Delay 1 second

 

    /* USER CODE END WHILE */

 

    /* USER CODE BEGIN 3 */

  }

  /* USER CODE END 3 */

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0