STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! No ST-Link Detected

I want to program my STM32WB55VG-Q6, but have been getting 'No ST-Link Detected'. I was using a Nucleo board previously and the ST-Link works fine with it. I am able to debug and flash the program onto the Nucleo but not on the STM32WB55VG-Q6 board. ...

lana5_0-1716803656849.png
lana5 by Associate
  • 1953 Views
  • 3 replies
  • 1 kudos

memory usage in stm32

Hi community!I write a simple code in stm32 and I need to calculate the memory usage from the build analyzer this is a part of the code   #define N 16146 volatile uint16_t adc_buffer[N]; int main(void) { HAL_Init(); SystemClock_Config(); MX_GPIO_Init...

toufik_iddou_0-1716736493013.png toufik_iddou_1-1716736558438.png

CubeIDE - SCB.CCR address for 'F0 (Cortex-M0)

While trying to help with a problem on STM32F030, I've noticed this:the address of SCB.CCR is 0xE000ED14; and the displayed value is wrong, too, as it's a read-only register with fixed value of 0x0208 (see ARMv6M ARM p.B3-228 - characteristically, th...

waclawekjan_0-1716643090171.png

Resolved! CubeIDE Issue - H755 LDO/SMPS settings missing

Hello,I have found a strong isssue in:STM32CubeIDEVersion: 1.15.1Build: 21094_20240412_1041 (UTC)(C) 2024 STMicroelectronics ALL RIGHTS RESERVEDThe IOC configurator for the STM32H755 lacks an option in the RCC configurationPower Parameters -> SupplyS...

zeboss49 by Associate III
  • 4726 Views
  • 5 replies
  • 0 kudos

Resolved! Interrupt behavior and its priority

Hello,I have a basic question regarding timer behavior in STM32.I have a common callback function HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) that handles timer interrupts at defined periods. I have set different priorities for timer globa...

PPate.9 by Associate II
  • 3595 Views
  • 2 replies
  • 3 kudos

Resolved! LED BLINKING in EMBEDDED C

I built a project in STM32F411E-DISC . project is built successfully and also  when we debugged no issue is found ,but after debugging only ORANGE LED is toggling rest 3 LED is not toggling . kindly help me to resolve this issue .kindly  find for cod...

WhatsApp Image 2024-05-21 at 11.16.40 AM.jpeg Capture-3.PNG Capture-2.PNG Capture-1.PNG
arunoday by Associate II
  • 10286 Views
  • 9 replies
  • 1 kudos

Resolved! Code generation issue after migrating from 1.14.1 to 1.15.1

 Hi, I had migrated my project from 1.14.1 to 1.15.1.When I change PSC on TIM17 from 0 to 99 on IDE and regenerate the code. The PSC value remains unchanged on tim.c, is this a bug or something I need to configure after migration?This is really annoy...

Philip0107_0-1716457510791.png Philip0107_2-1716457678736.png

Resolved! STM32CubeIDE after Upgrade ioc viewer changed

I upgraded stm32cubeIDE about a month ago, but since then, the readability of the theme has become very poor when looking at the ioc file. Can I revert to the previous one? Befire  After 

yolominwoo_4-1716523761956.png yolominwoo_2-1716523712025.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.