2020-02-07 4:24 PM
I am citing this error here, just in case someone else has this type of occurrence.
uint8_t data1[5];
for(uint8_t x = 0; x < 8; x++)
{
data1[x] = 0;
}When using an array in a count loop above the limits of the array, the compiler can report a warning:
warning: iteration 5 invokes undefined behaviorBut if pointers are used, the compiler may not warn and the program may enter an infinite loop:
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
CH10 data1 = 10
.
.
.Since the expected operation should look something like this:
CH0 data1 = 10
CH1 data1 = 10
CH2 data1 = 10
CH3 data1 = 10
CH4 data1 = 10
CH5 data1 = 10
CH6 data1 = 10
CH7 data1 = 10The code that caused the loop:
/* USER CODE BEGIN 0 */
uint8_t foo1(uint8_t *data2)
{
uint8_t data3[8];
foo2(data3, 0);
*data2 = data3[0];
return 0;
}
uint8_t foo2(uint8_t* data4, uint8_t channel)
{
for (uint8_t i = 0; i < 9; i++)
{
data4[i] = 10;
}
return 0;
}
/* USER CODE END 0 */
/* USER CODE BEGIN 2 */
for(uint8_t x = 0; x < 8; x++)
{
uint8_t data1 = 0;
foo1(&data1);
UsrLog("CH%d data1 = %d", x, data1);
HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);
HAL_Delay(500);
}
/* USER CODE END 2 */Note that the function foo1 passes an array[8] and the function foo2 tries to work with an array with 9 elements.
uint8_t foo1(uint8_t *data2)
{
uint8_t data3[8]; <-------- limit: 8
foo2(data3, 0);
*data2 = data3[0];
return 0; // error
}
uint8_t foo2(uint8_t* data4, uint8_t channel)
{
for (uint8_t i = 0; i < 9; i++) <----- limit: 9
{
data4[i] = 10;
}
return 0;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.