STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Why can't I install Segger JLink Utilities?

There is a big issue I'm facing. I just installed STM32CubeIDE 1.2.0 but then I get an error when trying to install JLink_Linux_V662_x86_64.debI absolutely need those tools because I also do development for other boards with Segger JLink probes.What ...

0690X00000Bx9WXQAZ.png
m4l490n by Senior
  • 6545 Views
  • 4 replies
  • 1 kudos

how write c++ and include c++ lib in stm32CubeIDE?

hiin stm32CubeIDE c++ code and standard lib (#include <iostream> or #include <iostraem.h>) not work.i test:'convert C to C++'make c++ projectuse only c++ code in func main() ==> 'bool a = true;' all test not woke!!!ya khoda

kshin.111 by Associate III
  • 3208 Views
  • 3 replies
  • 0 kudos

[Solved] Infinite loop without "Warning: iteration N invokes undefined behavior", using pointers to get data from a function

I am citing this error here, just in case someone else has this type of occurrence.uint8_t data1[5];   for(uint8_t x = 0; x < 8; x++) { data1[x] = 0; }When using an array in a count loop above the limits of the array, the compiler can report a warni...

by Not applicable
  • 4026 Views
  • 0 replies
  • 0 kudos

Hi everyone Why the generated code is not stable?

I am using STM32cubeIDE and STM32f103ret6 chip on my board The schematic I used is here: https://github.com/mcauser/BLUE_BUTTON_F103RET6/blob/master/docs/STM32F103RET6_schematics.pdf​I have two problems the NRST after some time _between 5 minutes to ...

Mugtaba by Associate II
  • 3472 Views
  • 6 replies
  • 0 kudos

Can I recover source code after accidental deletion.

I wanted to copy my project and start a new project based on this old project. In STM32CubeIDE, I right clicked on the project in the Project Explorer and chose copy and then pasted it back in. Somehow in the process of doing this or one step further...

Snom1 by Associate II
  • 1396 Views
  • 2 replies
  • 0 kudos

Can BUS Priority?!?

Hello everyone,I need assistance or any possible solutions in tackling this problem. I have a Nucleo F413zh, connected to three transceivers. They all work (yay!), however one of them doesn't receive messages properly but transmits properly! All of t...

WNguy.1 by Associate II
  • 2254 Views
  • 1 replies
  • 0 kudos

Is there a directive to demarcate the user code entered?

Device Configuration Tool Code Generation performs a code update, and if the user enters a code in an unmarked location, that code will be deleted.Is there a directive (something like #codeuser #endcodeuser) to demarcate the user code entered?

by Not applicable
  • 1746 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.