2025-04-14 2:33 PM
This is the thing: when I save the value 25 for the year, the built-in RTC saves the value 37 when the time saving precedes the date saving:
rtc.set_time( time );
rtc.set_date( date ); // it calls HAL_RTC_SetDate( this->rtc_, &rtc_date, RTC_FORMAT_BIN )So in my display (supposing today's date) it's printed: 14/04/37 (dd/mm/yy).
However, when I called the saving functions swapped I get the correct year:
rtc.set_date( date );
rtc.set_time( time );In my display it's printed: 14/04/25.
And it only happens with the year: day, month and weekday are written as expected. It seems that the HAL's function that make the conversion from binary to BCD is working also as expected:
/**
* @brief Convert a 2 digit decimal to BCD format.
* @PAram Value Byte to be converted
* @retval Converted byte
*/
uint8_t RTC_ByteToBcd2(uint8_t Value)
{
uint32_t bcdhigh = 0U;
uint8_t Param = Value;
while(Param >= 10U)
{
bcdhigh++;
Param -= 10U;
}
return ((uint8_t)(bcdhigh << 4U) | Param);
}
I was already aware that reading from the RTC must follow this pattern: read first the date and then read the time. Does this same bug applies also for writing? (Years ago this missbehavior was considered a bug, later on ST change its status to "by design", and the bug has been spread out among a lot of families).
Greetings!
2025-04-14 5:00 PM
> I was already aware that reading from the RTC must follow this pattern: read first the date and then read the time.
You must read time first, then date.
This is intentional to keep the time+date consistent and avoid a race condition.
> Does this same bug applies also for writing?
No, but because the date may tick over, you should set time first, then date. As long as it takes under a second to complete, it will work.
> This is the thing: when I save the value 25 for the year, the built-in RTC saves the value 37 when the time saving precedes the date saving:
Maybe provide a complete example showing the problem. The source code is inspectable. Unlikely to be a glaring error in a common peripheral that has gone unnoticed for years.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.