2025-09-29 7:47 AM
Hello, I have an stm processor (stm32h7b3zitx) connected to an ST Link V3 that is on an ubuntu server. My goal is to connect to the ST Link and run a remote debugging session from my windows laptop running the stm32CubeIDE. To accomplish this I have been running st-util -v -p 61234 on the ubuntu server and using the following debugging configuration in the cube ide.
I am port forwarding via an ssh connection to expose port 61234 on my windows machine. When I go to debug, I get the following error
I've attached the verbose gdb log from host machine and the verbose st-util log from the ubuntu server to this post. I'm wondering what steps I can take to resolve this. Thanks in advanced to all who view this!
Solved! Go to Solution.
2025-09-29 10:18 AM
Im not ubuntu expert, but on windows i use com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.6.0.202101291314 for remote dubuging with used big complicated config.txt. Plus firewall open.
2025-09-29 10:04 AM
Hello @stmAdmin
Is it detected with STM32CubeProgrammer?
Try connecting with STM32CubeProgrammer. Try mass erase, full chip erase, then try flashing.
2025-09-29 10:11 AM
Hi @Imen.D ,
The device is detected by stm32CubeProgrammer, here is the output from running STM32_Programmer_CLI -c port=SWD.
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 003E00293234510537333934
ST-LINK FW : V3J16M9B5S1
Board : STLINK-V3SET
Voltage : 3.26V
SWD freq : 8000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x480
Revision ID : Rev X
Device name : STM32H7A/B
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x92
2025-09-29 10:18 AM
Im not ubuntu expert, but on windows i use com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.6.0.202101291314 for remote dubuging with used big complicated config.txt. Plus firewall open.
2025-09-29 10:31 AM
Thanks @MM..1 !! Using the linux equivalent (/opt/st/stm32cubeide_1.19.0/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.linux64_2.2.200.202505060755/tools/bin) I am able to connect and debug!! I had tried this before, but without using the info from config.txt, I needed to add the -d flag to connect in SWD mode so thank you for mentioning the config. @Imen.D I'd still like to know why this doesn't work with st-util since it's advertised as being capable of this functionality, but I'm going to mark this one as solved!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.