2025-09-29 7:46 AM - edited 2025-09-29 7:51 AM
I'm looking for a way to have cubeIDE read from a .bin or .txt file on windows 11 and insert it's contents into a string array in my code during the build process.
So, if we have a file called "file.bin" stored somewhere on windows.
and inside this file we have "Text from file.bin"
In our code we have
unsigned char string[];
After build we have
unsigned char string[] = "Text from file.bin"
Solved! Go to Solution.
2025-09-29 8:09 AM - edited 2025-09-29 8:41 AM
Hello,
Maybe by using the prebuild feature and develop a script that reads that "file.bin" and updates your .c file?
2025-09-29 8:09 AM - edited 2025-09-29 8:41 AM
Hello,
Maybe by using the prebuild feature and develop a script that reads that "file.bin" and updates your .c file?
2025-09-29 8:34 AM - edited 2025-09-29 8:36 AM
For this purpose I have a small (quite old) C++ program bin2c.cpp, which reads a file and generates initialization for a C array from it.
So from your sample file it would generate:
klwa4731@eso22169:~$ cat > file.bin
"Text from file.bin"
klwa4731@eso22169:~$ bin2c file.bin
klwa4731@eso22169:~$ cat file.bin.c
// file.bin.c
// generated 29.09.2025 17:16:57 from file.bin
// by /usb1/klaus/projekte/bin2c.cpp $Id: bin2c.cpp 2013 2023-12-10 06:37:28Z klaus $
'\"', 'T', 'e', 'x', 't', ' ', 'f', 'r', 'o', 'm', ' ', 'f', 'i', 'l', 'e', '.',
'b', 'i', 'n', '\"', 0x0a,
// (21 bytes written)The generated file can be included in your C code like this:
...
unsigned char mystring[] =
{
#include "file.bin.c"
'\0'
};
...
A bit different is a similiar program bin2esc.cpp. It converts a file to an escape sequence. With option -p it changes to a printable string.
(The forum SW here fails to display an example output because of the escape sequences.)
You can use the output with #include... again.
There are many programs out there like these...
2025-09-29 8:38 AM
@mfgkw wrote:The generated file can be included in your C code like this:.
Or just have your C++ program generate a complete C source file, and include that in your Project.
Similar to this.
2025-09-29 8:56 AM
true, but I have no excel :)
2025-09-29 9:35 AM
I think i'll go with a Python script. Thank you!
2025-09-29 9:48 AM
I did say similar - you can do the same in any other programming language.
It's just a matter of emitting text.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.